cancel
Showing results for 
Search instead for 
Did you mean: 

Platform selection for new drone survey device

Justin1
Senior

Hi,

 I am helping establish a reliable drone survey product, performing low-bandwidth sense operations and image detection for on-board analytics. This unit responds to what it reports, performing control & maintenance when needed.

Unit:

- Drone w/steer & control`

- Image capture & analysis

- General sense, comm(RF/BT) & GPS

- Low power (e.g. for the proc, ~4-6 hours on 2000mAh?)

Services:

- Route Navigation

- Obstacle detection & avoidance

- Survey Image Analytics (AI request)

- Liquid dispense on request

- System network integration

This team has selected the Raspberry Pi 4 for solution, with interest in the Google Coral but I grew concern over reliable full-feature set support. Would the STM32MP support this feature set for a drone? They may ask for Google TPU support (the Coral's AI-engine via PCIe), would the STM32MP support interface to the TPU via PCIe?

It looks like the answer is a strong yes to all listed above, I was reaching out to you first for confirmation =)

Kind Regards,

 Justin

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0