Dear @Martin KJELDSEN, thanks for the update.Sadly not the one I wanted to hear :sad_but_relieved_face: So no easy path to have one team of firmware programmers create a GUIs on Cortex-M (STM32(F2/4)/F7/H7) and Cortex-A (STM32MP1) devices.Within o...
Dear @Martin KJELDSEN, any news on if we can expect support for TouchGFX WITH hardware acceleration running on STM32MP1 on-top of Linux next year?I'll have a project early next year where this would really help turn the tide in favor of the STM32MP1...
Hello @Martin KJELDSEN !Just wanted to know if TouchGFX support for STM32MP1 (running on Cortex-A on top of Linux Kernel, NOT Cortex-M), supporting all acceleration features of the platform, made it onto the TouchGFX roadmap?If yes, when is it plann...