cancel
Showing results for 
Search instead for 
Did you mean: 

ADC input protection on STM32MP157C

NGajic
Associate III

Hi,

I'm interested if there is ADC input protection against voltage transients and overvoltage inside STM32MP157C or I should add external protection for used pins? If I had to add external components do you have some recommendations?

Best regards,

Nenad

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hi,

ADC inputs are protected as other IOs (i.e. 5V tolerant if VDD and VDDA are present). Exception is ANA0 and ANA1 which are 'only' tolerant to 3.9V.

ESD is same for all, and specified in datasheet.

Protection are usually not present on ADC as analog inputs does not go directly outside of the PCB (there is always some circuitry) and so, are not prone to strong ESD stress.

Nevertheless, it depend on your application and system circuitry.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NGajic
Associate III

@[PatrickF] ,

​

Thanx for the answer, we will add some circuitry for ADC inputs.

​

Best regards,

​

Nenad​