STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OTA Update partitioning scheme

Hi,I am trying to integrate swupdate for OTA update integration for STM32MP1.In the due process I will be in need to modify the flash layout file a bit , since I am trying have an extra rootfs partition , named partition B on /dev/mmcblkp06.I referre...

NPal.2 by Senior
  • 1201 Views
  • 2 replies
  • 0 kudos

Resolved! DFU Broken after STLink upgrade (FIXED)

IDE suggested that I upgrade STLink FW on my STM32MP1-DK2 discovery board. Now when I connect my Linux PC to USBC on DK2, device isn't recognized by STMProgrammer (also nothing shows up in dmesg).

BBeck.1 by Associate II
  • 693 Views
  • 3 replies
  • 0 kudos

Interprocess communication buffer swapping

Hello,I am working on IPC between M4 and A7 and it works properly using the "logic analyzer" example. I changed it according to my needs but not the buffers. 1 . I could read the data from 3 buffers, but often buffers are swapping. I would like to wh...

JSIGA.1 by Associate II
  • 1277 Views
  • 4 replies
  • 0 kudos

Season's Greetings !!

Hi STM32 MPU's community ! On behalf of ST and all ST employees involved in this community I would like to wish - to all members here - a joyful holidays period and the best for coming year 2022 !I take this opportunity to thanks you all for your par...

0693W00000HoxMYQAZ.png

How to troubleshoot remoteproc on STM32MP157C.

I am getting an error in the kernel log when remoteproc tries to "set hold boot" during startup in Linux. The error is:remoteproc remoteproc0: failed to set hold bootremoteproc remoteproc0: releasing m4stm32-rproc: probe of mlahb:m4@10000000 failed w...

PZak.1 by Associate III
  • 2147 Views
  • 5 replies
  • 0 kudos

Resolved! Ecosystem 3.1.11: Patch real-time kernel for linux-5-10-61

Hi allFor test purpose I want to run a real-time kernel on the STM32MP157c-DK2 with the newest ecosystem 3-1-11. The goal is to develop a real-time kernel module, out of the Yocto environment.I did build the Image with Yocto and flashed the image. Ap...

Led by Senior
  • 915 Views
  • 2 replies
  • 0 kudos