cancel
Showing results for 
Search instead for 
Did you mean: 

OTA Update partitioning scheme

NPal.2
Senior

Hi,

I am trying to integrate swupdate for OTA update integration for STM32MP1.

In the due process I will be in need to modify the flash layout file a bit , since I am trying have an extra rootfs partition , named partition B on /dev/mmcblkp06.

I referred to flash layout currently mentioned here.

It looks to me that there is not any support for the extra rootfs which is provided.

How can i do that?

I am sure that I will be in need to change the flashlayout but since offsets are defined static in the mentioned link , I was wondering what should be offset calculation for achieving the same.

I want to achieve following scheme:

#Opt    Id      Name    Type    IP      Offset  Binary
-       0x01    fsbl1-boot      Binary  none    0x0     arm-trusted-firmware/tf-a-stm32mp157c-ev1-usb.stm32
-       0x03    fip-boot        Binary  none    0x0     fip/fip-stm32mp157c-ev1-trusted.bin
P       0x04    fsbl1   Binary  mmc1    boot1   arm-trusted-firmware/tf-a-stm32mp157c-ev1-emmc.stm32
P       0x05    fsbl2   Binary  mmc1    boot2   arm-trusted-firmware/tf-a-stm32mp157c-ev1-emmc.stm32
PD      0x06    fip     Binary  mmc1    0x00080000      fip/fip-stm32mp157c-ev1-trusted.bin
P       0x10    boot    System  mmc1    0x00480000      st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P       0x11    vendorfs        FileSystem      mmc1    0x04480000      st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P       0x12    rootfs  FileSystem      mmc1    0x05480000      st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x13    rootfs2  FileSystem      mmc1   ??????????     st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x14    userfs  FileSystem      mmc1    ??????????      st-image-userfs-openstlinux-weston-stm32mp1.ext4

What shall be value at the place where I have mentioned ----> "??????????"

TIA

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @NPal.2​ ,

You can customized the flashlayout as per your need since you respect the recommendation for partition size

STM32CubeProgrammer flashlayout - stm32mpu

Offset is just the addition of each partition size.

The flashlayout on wiki allocate 746MB to rootfs ( you can change it )

So if you want to double it, it would give something like :

P       0x12    rootfs  FileSystem      mmc1    0x05480000      st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x13    rootfs2  FileSystem      mmc1   0x33E80000     st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x14    userfs  FileSystem      mmc1    0x62880000      st-image-userfs-openstlinux-weston-stm32mp1.ext4

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @NPal.2​ ,

You can customized the flashlayout as per your need since you respect the recommendation for partition size

STM32CubeProgrammer flashlayout - stm32mpu

Offset is just the addition of each partition size.

The flashlayout on wiki allocate 746MB to rootfs ( you can change it )

So if you want to double it, it would give something like :

P       0x12    rootfs  FileSystem      mmc1    0x05480000      st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x13    rootfs2  FileSystem      mmc1   0x33E80000     st-image-weston-openstlinux-weston-stm32mp1.ext4
P       0x14    userfs  FileSystem      mmc1    0x62880000      st-image-userfs-openstlinux-weston-stm32mp1.ext4

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Community member​ : Thanks for the response. I just modified few set of things in the file :

./meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc

Added below lines :

ROOTFS2_PARTITION_SIZE ?= "${IMAGE_ROOTFS_MAXSIZE}"
 PARTITIONS_CONFIG[rootfs2]  ?= "${IMAGE_BASENAME},rootfs2,,${ROOTFS_PARTITION_SIZE},FileSystem"

with I got the flashlayout generated according to my need.

Thanks for the inputs.