Skip to main content
PZak.1
Associate II
December 10, 2021
Question

How to troubleshoot remoteproc on STM32MP157C.

  • December 10, 2021
  • 5 replies
  • 3064 views

I am getting an error in the kernel log when remoteproc tries to "set hold boot" during startup in Linux. The error is:

remoteproc remoteproc0: failed to set hold boot

remoteproc remoteproc0: releasing m4

stm32-rproc: probe of mlahb:m4@10000000 failed with error -3

After this I do not have remoteproc0 in the /sys/class/remoteproc folder. I have attached device tree and log file.

Can someone please suggest a possible cause.

This topic has been closed for replies.

5 replies

ArnaudP
ST Employee
December 15, 2021

Hello,

The following log message shows that you are not use the good version of the Linux Kernel:

"remoteproc remoteproc0: failed to set hold boot"

At least following patch is missing:

https://github.com/STMicroelectronics/linux/commit/ce92c44d652b44ef0967a8b8d2f9979105bf64f6#diff-5ca23cfd6108ec38be554f2240b3f3a23e60fed01d21dde9672b91bc4092e7ce

Please use the Linux kernel provided in the ST Microelectronics distribution

For the Linux Kernel 5.4: https://github.com/STMicroelectronics/linux/tree/v5.4-stm32mp

PZak.1
PZak.1Author
Associate II
December 16, 2021

Hello Arnaud,

Thank you for responding. I tried the patch you supplied but remoteproc failed with the following error:

stm32-rproc: probe of mlahb:m4@10000000 failed with error -2.

We are using the Octavo systems OSD32MP15x SIP and can not easily update to the latest kernel version.

I have since found out that if I use the arm-trusted-firmware/tf-a-stm32mp157c-dk2-sdcard.stm32 binary provided by ST then the ARM SMCCC call that failed originally now succeeds and remoteproc0 is present in the file system. I will have to dig into what I am doing wrong in the TF-A build of our image.

Best regards,

Olivier GALLIEN
ST Technical Moderator
December 16, 2021

Hi @PZak.1​ ,

>> We are using the Octavo systems OSD32MP15x SIP and can not easily update to the latest kernel version.

For this I recommend you to get support from Octavo directly.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.