STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to convert init manager from sysvinit to systemd and run weston at startup in yocto project?

Using yocto project and changed default sysvinit to systemd with below line in local.confINIT_MANAGER = "systemd" DISTRO_FEATURES += "pam vulkan opengl egl wayland" CORE_IMAGE_EXTRA_INSTALL += "wayland weston" IMAGE_INSTALL:append = " chromium-ozone-...

Seenu by Associate II
  • 1565 Views
  • 1 replies
  • 0 kudos

STM32MP157C-DK2 flash didn't work.

I've tried to flash STM32MP157C-DK2 SDCard like described in ST wiki with command STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv.and it didn't work! i got following error report. it see...

RYin by Associate II
  • 4896 Views
  • 15 replies
  • 0 kudos

On VMWare's Ubuntu 20.04 LTS, the STM32 program tool is not associated with the STM32MP157D evaluation board.

Hello, teachers.​First, The board I am using is the STM32MP157D evaluation board.​I checked the article that the starter package can be installed in Windowsos, but the developer package and the distribution package are only available in the Linux env...

kKim.1 by Associate II
  • 2015 Views
  • 3 replies
  • 0 kudos

having trouble in configuring device tree for STM32MP157c based board by karo-electronics, QSMP1570 on qsbase2, having yocto kirkstone and kernel 5.15, where to find the macros to be used in dts files, because i am unable to bitbake after my change

I have a board from karo-electronics, STM32MP157c based QSMP 1570 SOM over qsbase2, I am trying to configure above mentioned board for my specific application, The distribution is build using yocto by karo-electronics, I am unable to edit the dts fil...

SChat.2 by Associate II
  • 1874 Views
  • 4 replies
  • 0 kudos