STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issues with crypto IP core

We have encountered a problem with CRYPTO IP core on STM32MP157C.Our setup is STM32MP157C-DK2 with latest image/SDK installed(openstlinux-5.10-dunfell-mp1-21-11-17).1. First of all, our IPSec solution based on strongSwan doesn't work atall when stm32...

dimax by Senior
  • 1681 Views
  • 4 replies
  • 0 kudos

Creating a flashable backup of sd card image

Hello, I have sd card with lots of things configured.To save time I want to create backup of this card which I can flash later.Is there any official way to take the backup of the STM32MPU sd card image and also a way to flash the same image on new SD...

darla14 by Senior
  • 419 Views
  • 2 replies
  • 0 kudos

Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong? Sincerely, Alexander.

Good afternoon, I have written two versions of the time output test programs to the console for STM32MP157D. Both programs work no more than 2 hours, then the system restarts. What did I do wrong?Sincerely, Alexander. ////////////////////////////////...

Vlaty.1 by Senior
  • 660 Views
  • 2 replies
  • 0 kudos

Resolved! How to disable Peripherals in stm32mp1 u boot source?

Hi,We are using stm32mp157a processor in my custom board.In my custom board we have limited peripherals so i need to disable remaining peripherals like ltdc and hdmi ,etc. I disabled in dts files but it didn't effected. How can i disable peripherals ...