STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't get out of DFU mode.

Hello,Using a custom board loosely based on STM32mp157F-DK2we are using boot0 and boot2 pins.According to documentation,boot mode configuration is as follows;Boot Mode     BOOT2  BOOT0Recov/DFU        0      0Nor              0      1Reser...

Resolved! how to use jtag in stm32mp157f-dk2

stm32mp157f-dk2 is not embedded jtag connector,but i want to use jtag debugger.​st-link(stm32f103cbt6) embedded in stm32mp157f-dk2 has jtag pin(T_JTCK, T_NRST, T_SWO, T_JTMS)Q1. Can't I use jtag with only ST-LINK USB CONNECTOR (5 pin)?Q2. what should...

0693W00000bhLyaQAE.png
SKim.36 by Associate II
  • 4309 Views
  • 5 replies
  • 0 kudos

Good afternoon! I'm trying to use TSC2046 based touchscreen device on a STM32MP157C-DK2 based custom board. I get SPI transfer time-out when touching the screen. Does anyone have a similar problem ?

I'm using spi5 and my device tree settings are &spi5 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&spi5_pins_a>; pinctrl-1 = <&spi5_sleep_pins_a>;    #address-cells = <1>;    #size-cells = <0>; num-cs = <1>; is-decoded-cs = <0>; cs-gpios = <&gp...

Ronte.1 by Associate III
  • 3742 Views
  • 4 replies
  • 0 kudos

How to enable PWR_USB_SW in STPMIC?

Hello,I am working on a custom board based on stm32mp157 and I have the need to enable the PWR_USB_SW through the ST PMIC. So far, I identified the bit VBUSOTG_ON in register BST_SW_CR (0x40) but I had no success in configuring it via devicetree or v...

bimorqt by Associate III
  • 5359 Views
  • 9 replies
  • 0 kudos

when i use STMCubeMX(version6.8.0) to generate the code about STM32MP157DAA1,i find whether i define the GPIO's user label,it just can't generate in the keil project.

i also find some people say this is a bug,repeatedly click the setting of user label can be solved,but i try it's can‘t figure it out.....By the way,GPT also not give the correct solution (this is why i am here)​this is my first question in this com...

GGree.2 by Associate II
  • 2573 Views
  • 4 replies
  • 0 kudos

Resolved! cube mx does not launch workspaces

Greetings,in the video STM32MP1 workshop - 9 OpenSTLinux BSP pin Muxing - STM32CubeMX lab after modifying the DK2_TIMER_A7 project in the mx cube directly open the project in workbench from generate code, open the file.On my pc this doesn't happen, t...

MMarc.11 by Associate II
  • 6392 Views
  • 4 replies
  • 0 kudos