Skip to main content
DGree.2
Associate II
February 11, 2022
Solved

Is single NOR Flash boot supported by the STM32MP15xxAD (TFBGA257 package)?

  • February 11, 2022
  • 4 replies
  • 1606 views

According to the wiki here: Boot from serial NOR, the pins required to boot from a serial NOR flash chip in single mode are PB6, PF8, PF9, PF10. These pins are present on the TFBGA257 package. To boot in dual mode, PH2 and PH3 are required, and these pins are *not* present on the TFBGA257 package. So from this, it seems this package supports serial NOR flash booting in single mode only.

However, CubeMX does not let me enable the QUADSPI peripheral for BOOTROM. If I try, it highlights all the choices in red and gives the error message: "Pin not available for boot step (boot ROM)".

So, is this a bug in CubeMX, or does this package not support single-chip NOR Flash booting? I'm re-designing a board to use this chip instead of a larger package, and we require serial NOR flash booting. So it'd be good to know before committing to the design.

thanks

Dan

This topic has been closed for replies.
Best answer by OlivierK

I wouldn't worry too much because there's the same behaviour with the BGA 448 package. So it is not a pin limitation but rather a quirk of CubeMx.

4 replies

OlivierK
ST Technical Moderator
February 14, 2022

Hello DGree.2 (Community Member)

Indeed PB6, PF8, PF9, PF10 are present on the TFBGA257 package for serial NOR flash in single mode.

In Cube Mx v6.4, the STM32mp157CADx for instance (TFBGA257 package) QSPI is available and "boot rom" box can be ticked (no red choices, only yellow since dual is not possible in this package)

0693W00000JPhdgQAD.jpg 

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DGree.2
DGree.2Author
Associate II
February 14, 2022

In your screenshot you have "A7NS (Linux)" checked. If you uncheck that and just check "Boot ROM" then the choices turn red. As soon as you select "A7NS (Linux)", then some choices are yellow like in your screen shot. But if you just check Boot ROM, then all choices are red or grey.

Is this just a bug or odd quirk of CubeMX?

Or does this imply I cannot boot onto NOR Flash with this package? I've poured over the relevant sections in the TRM but see nothing about limitations on serial NOR Flash booting for certain packages. Obviously there are limitations since this package lacks the pins to do dual serial NOR flash booting. So I'm wondering if this information is just missing from the TRM, or if CubeMX has a bug.

See screenshot.

0693W00000JPkGLQA1.png

OlivierK
OlivierKBest answer
ST Technical Moderator
February 14, 2022

I wouldn't worry too much because there's the same behaviour with the BGA 448 package. So it is not a pin limitation but rather a quirk of CubeMx.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DGree.2
DGree.2Author
Associate II
February 14, 2022

Ok, thanks for the re-assurance. Being so hard to acquire parts, we want to make sure we design for the right thing.