STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Interface can0 isn't appearing in STM32MP157F-DK2

I enabled CAN in the device tree using STM32CubeMX and followed the instructions in the provided documentation to generate the .dtb file. Afterward, I copied the generated .dtb file to the /boot directory. In the terminal, I ran the following command...

STM32MP157 Memory

Hi,I am designing a product based on the STM32MP157DAC specifically using the TFBGA257 package due to its compact size. I was just looking at the datasheet (page 16, Table 1) and noticed that under the SDRAM section it seems that this package doesn't...

TechSys by Associate
  • 212 Views
  • 2 replies
  • 0 kudos

STM32MP157 Memory Controller

Hi,i have a question to the memory-controller and the supported memory-size.I'm using the Part STM32MP157CAAx (Package: LFBGA448).In the Datasheet (STM32MP157C/F) and AN5031 there is a definition to the supported SDRAM size.For package "LFBGA448" the...

Fritz2 by Associate
  • 247 Views
  • 2 replies
  • 0 kudos

STM32MP157 custom board, linux build tutorial

Is there a tutorial for newbie? I made my custom board by myself as hobby.the board has switches to select boot 0 and boot 1, boot 2 is tied to ground through 10k resistor. so I could implement boot selector that switches between `00` flashing mode, ...

KakaoTalk_20250304_223414540.jpg KakaoTalk_20250304_223414540_01.jpg KakaoTalk_20250304_223414540_02.jpg KakaoTalk_20250304_223414540_03.jpg
jaehoon by Associate II
  • 345 Views
  • 2 replies
  • 1 kudos

Direct use of SDL with kms / drm

Hello,I use SDL with X11 for now but I want to use it directly with kms/drm kernel driver. I run basic_splash_drm and it works.I don't know how to configure sdl to work together with kms/drm, somebody use it in this way ?Regards,Adrian

Adrian1 by Associate III
  • 6370 Views
  • 3 replies
  • 2 kudos