User Activity

Hi,i have a question to the memory-controller and the supported memory-size.I'm using the Part STM32MP157CAAx (Package: LFBGA448).In the Datasheet (STM32MP157C/F) and AN5031 there is a definition to the supported SDRAM size.For package "LFBGA448" the...
Hi,I'm working on layout routing from STM32MC257AAK(Package: VFBGA424) to LPDDR4 (32bit).I have read the "Memory layout rules" in the App-Note AN5724.For a good LPDDR4 signal timing it is usefull to do a "Line-Length-Matching" on the LPDDR4 signals, ...
Kudos given to