cancel
Showing results for 
Search instead for 
Did you mean: 

Request for Recommendations on 64-bit ARM Development Boards

Vista123
Associate II

Hi,

I am looking to design a board based on a 64-bit ARM processor, with interfaces including USB, Serial, and Ethernet. Could you kindly suggest any development boards that could serve as a good reference for this project?

Your recommendations would be greatly appreciated.

 

Thank You

2 REPLIES 2
TDK
Super User

I believe this is the only 64-bit chip from ST:

STM32MP2 series - STMicroelectronics

 

Also on the way:

STM32MP25: 1st STM32 MPU with 1.35 TOPS NPU and 64-bit cores #STM32Summit

If you feel a post has answered your question, please click "Accept as Solution".
PatrickF
ST Employee

Hi @Vista123 

two development boards are available from ST

https://www.st.com/en/evaluation-tools/stm32mp257f-dk.html

https://www.st.com/en/evaluation-tools/stm32mp257f-ev1.html

See also https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards

 

note that such board are for evaluation/development and cannot be sold inside a product: https://www.st.com/resource/en/evaluation_board_terms_of_use/evaluationproductlicenseagreement.pdf

 

Some STM32MP2x boards (e.g. SOM modules) are available from partners or 3rd parties.

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.