Associate II
January 2, 2025
Solved
Interface can0 isn't appearing in STM32MP157F-DK2
- January 2, 2025
- 4 replies
- 998 views
I enabled CAN in the device tree using STM32CubeMX and followed the instructions in the provided documentation to generate the .dtb file. Afterward, I copied the generated .dtb file to the /boot directory. In the terminal, I ran the following commands:
sync
reboot
After rebooting, I checked the dmesg log and found the following output when filtering for CAN-related messages:
dmesg | grep can
[ 0.451665] can: controller area network core
[ 0.451819] can: raw protocol
[ 0.451832] can: broadcast manager protocol
[ 0.451847] can: netlink gateway - max_hops=1
However, when I checked the available network interfaces can0 isn't avaliable
root@stm32mp1-e1-99-00:~# ls /sys/class/net
end0 lo usb0 wlan0
I have attached the dts file for reference