STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Could not set DRM mode for screen DSI1/Could not queue DRM page flip on screen DSI1 (Permission denied) for st-example-image-qt

Hi,I have succesfully built a image st-example-image-qt from the DISTRO openstlinux-eglfs.I have deployed the image on sd card, and played it on STM32MP157C-DK2.System is booting without a problem, and the splashscreen was shown.Then, I tried one of ...

Resolved! DFU not detected

HiI got an STM32MP157C-DK2 during the Embedded World.But Windows7 isn't detecting the DFU ... It detects only the STLink (UART) ....Same issue in a Ubuntu-16 (which is running in VirtualBox on the same Windows 7)Any suggestion?Regards Francesco

Resolved! STM32MP1 Distribution package access rights

Hi,I'm planning to buy an STM32MP1 discovery kit (when available) and I'm wondering how to get access to the distribution package. I read on wiki.st.com that I have to request these rights to my ST support contact but I can't found out how to do it.T...

Silicio by Associate
  • 1126 Views
  • 2 replies
  • 0 kudos

Resolved! Yocto_SDK Software Version- 1.0.0 for STM32MP151C. Is it suitable for just raw framebuffer implementation?

I downloaded Yocto_SDK Software Version- 1.0.0 for STM32MP151C. The environment setup file name is - "environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi". Does it mean that this SDK is tailored for Wayland implementation? We i...