cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157 Memory

TechSys
Associate

Hi,

I am designing a product based on the STM32MP157DAC specifically using the TFBGA257 package due to its compact size. I was just looking at the datasheet (page 16, Table 1) and noticed that under the SDRAM section it seems that this package doesn't support 32 bit. I have trawled the internet for additional information to support this but can't find anything that might suggest this to be the case. Can anyone chime in if you've had any experience using this package or if you know of any additional literature.

 

Cheers,

2 REPLIES 2
Erwan SZYMANSKI
ST Employee

Hello @TechSys ,
As you mention it regarding the datasheet of your package, there is no support of 32-bit DDR3 for the TFBGA257 or LFBGA354 package.

You can also see in the DDR memory routing guidelines Application Note that this configuration is not supported.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

HI @TechSys 

Notice that STM32MP157DAC is TFBGA361 12x12mm (which support 16-bits and 32-bits DDR) whereas STM32MP157DAD is TFBGA257 10x10mm (which support 16-bits DDR only)

 

Anyway, you could start your design by looking at:

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.