Resolved! How about STEVAL-SMARTAG1?
I have learned that STEVAL-SMARTAG1 can power MCU through EH of ST25 to achieve wireless transmission function, then can I replace the digital sensor with a thermocouple as a principle to collect data?
I have learned that STEVAL-SMARTAG1 can power MCU through EH of ST25 to achieve wireless transmission function, then can I replace the digital sensor with a thermocouple as a principle to collect data?
Hi! I am a student new in this theme and i am searching for components to create a energy harvesting NFC system. This will work only with the power given by a mobile reader though the antenna. Searching for a dynamic tag, i have see that only M24LR a...
Hello, I don‘t understand the Syntax of the Function rfalWriteMultipleRegister(). After trying and don‘t receive any Data. Can someone provide an example on how to use the function. Thank you very much Rgds
Hi,In ST25RFAL library, version 2.8.0, in rfal_isoDep.c, function rfalIsoDepHandleControlMsg(), when ISODEP_S_WTX messages is handled, the code limits how many times a card can request wait time extension, specifically, this line: if( (gIsoDep.cntSW...
Hello,I am trying to create an application that is able to use the ST25R3911B-DISCO to read ISO15693 tags. I read on the forums and understand that the reader does not natively support ISO15693 tags but that there is a RFAL library created by ST whic...
Hi,I am assessing to use CR95HF, ST95HF or ST25R95 for a low power access control reader application and I have a question.I would like to know if thre is any difference between thse 2 parts:ST95HF ST25R95Regards, Ramon.
Hello everyone, I'm using the X-Nucleo-NFC08A1 and a Tag (ISO 15693). For my project I want to enable a Write Protection on Page 0(Blog 0-3) and Page 1(Block 4-7). Are their any applications or examples that show me how its done ? Thank you for your ...
Hi, In AN4974 (antenna matching network for ST29R391x device), In chapter 6.2.1 in Simulation S-parameter and Transition model, what is the tool used for simulation in this case?Best,Dalik
Hello everyone, I want to Read / Write a Tag using the X-Nucleo - NFC08A1. The demo project(polling) runs perfectly. I also installed X-Cube-NFC6. Which rfal libary is the best and how do I implement the function in the main.c. Tnak you for helping
Hi Everyone,I have implement this chip on my device and now i try to find tags LXMS21ACMF-218 from Murata. I have ported software from:https://www.st.com/en/development-tools/stsw-st25ru-sdk.htmland now i'm trying it with STUHFL_DEVICE_MODE set but w...