User Activity

Hello everyone, I m trying to create my own NFC-Reader Board with a ST25R3916B. With the help of the x-Nucleo NFC08A1I designed my own shematic. After ordering my custome curcit board and assembling all parts I tried to get it running but it does not...
 Hello everyone, for my project I am using the X-Nucleo-NFC08A1 board. In addition, I am using an external antenna that I operate differentially. The antenna is connected to the board via an SMA connector. I know that I should also adjust the matchin...
Hello everyone,I am using an NFC08A1 for my project and I would like to use the AAT. I roughly understand what happens in the AAT algorithm. However, I don't get any noticeable improvement when I apply it. The range in particular remains almost the s...
Hello everyone, for my project, I need to read a tag in two different places. Currently I am using an X-Nucleo-NFC08A1. I would like to add an additional X-Nucleo-NFC08A1 reader.The communication is done via SPI. What adjustments do I have to make in...
Hello everyone, for my project I need to enter the secure mode on a em4233 Glastag. I also use X-Cube-NFC6. The rfal-librarys only support tags from STM. I do not know how to send the command to the Tag can some explain or provide a example. Thanks 
Kudos from
Kudos given to