2023-09-11 8:42 PM
I have learned that STEVAL-SMARTAG1 can power MCU through EH of ST25 to achieve wireless transmission function, then can I replace the digital sensor with a thermocouple as a principle to collect data?
Solved! Go to Solution.
2023-10-24 10:14 AM
Hello,
the VDD_MEMS voltage is provided by the microcontroller through one of its GPIO. Therefore, the voltage is limited to 1.8 V. The MAX6675 thermocouple require a voltage range between 3.0 V to 5.5 V to operate, so it is not possible to use VDD_MEMS to power the MAX6675.
Best regards,
Michael
2023-09-26 5:06 AM
Hi,
pleas ehave a look at this post, this could answer your question :
Obtaining 3 axis data from LIS2DW12 using Steval-Smartag 1 board
Best Regards,
BB
2023-09-26 5:24 AM
Yes, but I have a question about the STEVAL-SMARTAG1, if I need to measure the temperature using the max6675 and thermocouple, can I utilize the power source obtained by VDD_MEMS?
2023-10-24 10:14 AM
Hello,
the VDD_MEMS voltage is provided by the microcontroller through one of its GPIO. Therefore, the voltage is limited to 1.8 V. The MAX6675 thermocouple require a voltage range between 3.0 V to 5.5 V to operate, so it is not possible to use VDD_MEMS to power the MAX6675.
Best regards,
Michael