Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IHM01A1 L6474 reset pin during active output

Posted on October 13, 2015 at 11:11 I have some question regarding the board (maybe anyone of you have a better understanding on electronic). I use the board with stepper motor to moves a cart on the linear drives. The move will be limited by proxim...

How does PWM timing work in L6470

Posted on September 03, 2015 at 13:50My question is a typical 1.8deg step motor (200 steps per rev) set for 128 micro steps will finish each micro step in <10usec at a speed of 300RPM. With a PWM period of 64us (15.625K) how this PWM can set a desir...

tejpal by Associate
  • 781 Views
  • 1 replies
  • 0 kudos

Viper06: documents for the compensation network design

Posted on November 14, 2012 at 15:15Hi, I'm just searching for some Viper06 documentation like some application note that explain-me how to design the compensation network. I just get some value with the online tool, but I'd like to understyand how ...

Viper06 over current

Posted on November 12, 2015 at 12:51Hello, I've done a Viper06LS based AC/DC converter. The criteria : full bridge ahead, 26V, 0.11 A out. I've designed it with the online tool, but the circuit is always in overcurrent (on 250ms then off 1s). Is t...

D.Cedric by Associate II
  • 769 Views
  • 0 replies
  • 0 kudos

Spice Model Viper26LD

Posted on November 06, 2015 at 14:11Hi,I would like simulate the viper26 on my application, but I do not found spice model. Could someone help me?Thanks

Slow Speed Motor Control

Posted on October 27, 2015 at 21:37I am having troubles controlling the speed of my motor below ~100 RPM (~10Hz on the halls). I am having similar issues with both Hall Effect and sensor-less modes. I could understand this being an issue with the se...

how to start using PMSM to write FOC ?

Posted on October 21, 2015 at 07:32I downloaded the PMSM Motor Example. I want to fix my own programs, but has no idea .I just wanted to ask if the external input from ia, ib, via FOC algorithm, the output value of the three-phase voltage to the osc...

Brake for on-the-fly start-up

Posted on October 28, 2015 at 19:46Hi, According to the user manual UM1080 p.16, ''The duration of the ''braking phase'' that is applied if the sensorless measurements doesn't give reliable measurement during the ''detection phase''. During the ''br...

KF Lam by Associate II
  • 1464 Views
  • 2 replies
  • 0 kudos

Non-detected Stall L6474

Posted on October 20, 2015 at 14:44I am working  a bipolar stepper motor against a spring to assess the torque delivered. The test drives a set distance and then returns. Software produces a constant accel profile in incremental steps of pulse rate....

estie by Associate II
  • 666 Views
  • 0 replies
  • 0 kudos