export classification ST23YS08
Can someone/anyone confirm the U.S. ECCN for ST23YS08, Smartcard MCU with Enhanced Security and 8 KBytes High-Density EEPROM?
Can someone/anyone confirm the U.S. ECCN for ST23YS08, Smartcard MCU with Enhanced Security and 8 KBytes High-Density EEPROM?
*Is it possible to utilize just one phase from the SLLIMM high-power IPM, which is a 3-phase inverter with a 650V short-circuit rugged IGBT rated at 50A? Additionally, do you have an IPM comparable to the discontinued STGIPS40W60L1, a half-bridge IGB...
I'm trying to get started with the STUSB4500QTR and at this point have not changed anything in the device but at the same time I am not using any of its capabilities. The attached schematic shows where I am now. The intent is that a PC (right now jus...
The LSM303AHTR sensor is housed in an enclosure and that vibration is limited due to the stability of the housing. During windy condition the sensor constantly transmit false signals even though there was little to no movement to the Accelerometer an...
Hello to the ST engineers or anyone familiar with problems when programming the STSAFE devices: We are seeing about 10% of our STSAFE-A110 devices permanently fail during initial programming. Per the guidance in Section 5.2 of the data sheet (linked ...
Is there FIT data available for STPS30170DJF Schottky Diodes? Best regards, Martin Best
I am looking for EOL data, tolerance, and thermal Variance.Any info would be helpful.Thank You.
Hi, I wonder if the analog switch STG3692 can be used with +5V. I have concerns because recommended voltage value is +4.3V in the datasheet while absolute maximum is +5.5V, is there any risks about thermal conditions at that level? What do you sugges...
i am working with black pill board that uses stm32f401ccand i have a debugger that was attached to neucleo board stm32f401re and i broke it from the board , the black bill debug pins only have the ground and the 3.3 and the swsck and the swdio ,i co...
Hi, Im trying to track down a couple of diodes to repair a card. The markings are EV Z551 It also has the ST logo on it, surface mount.. Anyone know where I can obtain some.. Cheers Kev