LSM9DS1 provides 3 orientation registers (ORIENT_CFG_G), but I need Euler angles instead and conversion algorithms require four orientation values. Could you help?
The below mentioned parts are failing for the ISO 7637-2 Pulse 5a and 5b. I have attached the image of the simulation result which we have done for the ISO 7637-2 pulse 5a in that the maximum power is went beyond the rated power of SM6T39CAY TVS diod...
Hello everybody!Wish y´all a good day, i´m considering to use the STRKT01 for a project but before i buy it i need to know the physical dimensions of the module/development card, also the dimensions of the case that the kit includes. Thanks!
Question from MOhamed_Mehery, moved to mcu-wireless-forum
We are using VN5T006ASP-E in our project. I need to know How to find the whether the IC (VN5T006ASP-E) falls below which of the category CMOS/BICMOS/BIPOLAR?In general, suggest a common technique to find the IC fabrication technology?
We are using S2-LP Transceiver to wireless products of us. Our custom board has 2 layer and 1.6mm thickness and our operating frequency(OP) is 868 MHz. Also our output power is 14dBmUnfortunately we failed "Unwanted Emission in Spurious Domain" test....
I want to simulate clt01_38q7 with LTSpice, but I couldn't find the spice mode in cad resources, so could you please provide it?
Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °Cbut ST72F561J9TBXS Datasheet not mentioned suffix B temperature range, could you please share? thanks!