M93C56-WDW6TP
Hello!Please tell me what the letter K means in the first line of the C56WK marking?My colleagues say that the ending can be either P or G. The Chinese supplier sent a photo before purchasing.We need 4 psc.Thank you!Best regards, Jack
Hello!Please tell me what the letter K means in the first line of the C56WK marking?My colleagues say that the ending can be either P or G. The Chinese supplier sent a photo before purchasing.We need 4 psc.Thank you!Best regards, Jack
Hi, I am trying to get more info on what I believe is EEPROM chip, it is in Haldex 5th generation and trying to find same or similar replacement, as I have more and more faulty, corroded units that I could repair.Any help welcome, Thanks all
Previous I2C EEPROM chips had (eg) 3 address pins A2..A0, where you could hardware the I2C address. This allowed up to 8 devices on the same I2C bus in case you need more storage capacity.With the M24M01E this is no longer the case : the device can h...
M95M02-DRMN6TPMay I ask if there are any cases that cannot be EEPROM programming that can be shared?We are unable to EEPROM programming,thank you
Hi,Why is there no RAM block inside the Block diagram?In the document AN5747 (Page EEPROM memory architecture) there is a RAM block mentioned, but in the block diagram from the M95P32 datasheet no RAM block is available/visible.Thanks in advancenobod...
您好M95M02-DRMN6TP 请问有 DEMO资料分享下吗这个物料 烧录不进 请问有没有案列分享下呢谢谢!
the chip of ST is different from traditional manufacturers that use circular dot or gap to distinguish the first pin of the IC. I cannot find the information in datasheet or the topics. Anyone can give me some information? thanks very much
Hi,Why is the page-write consuming less power then a page-program? When I understand it correctly then the page-write, is first erasing the page and then writes the values back. So then the page-write power consumption should be similar to erase and ...
Hi, We have made a custom development board integrated with M24M01E-FMN6TP EEPROM IC. It is operating at 1.8. Having queries like whether the supply voltage plays a role in accessing total pages of EEPROM and if so please tell us the minimum voltage ...
Hello, I am looking for the IBIS model of EEPROM (M95020-WDW6TP) for the SI analysis. Do you have it available?Please let me know.