EMIF02-USB03F2 replacement
Hello, This component, EMIF02-USB03F2, is listed as EOL. Do you have a direct/indirect replacement?Thanks,
Hello, This component, EMIF02-USB03F2, is listed as EOL. Do you have a direct/indirect replacement?Thanks,
Need Prop65 Certificate for STM32F413RGT6511-USBLC6-2SC6
Hey everyone!I am trying to understand the snubber design for a 3 phase inverter to reduce ringing. What is the difference between placing the RC snubber:- between each phase output and ground (3x RC snubber)- between drain and source of every mosfet...
Hi, I am using LSM6DSO IMU sensor to track motion and need to know the specifications of the inbuild Low pass filters. Datasheet only shows the block diagram and does not provide any information about filter type, order, frequency response. Could you...
ECMF2-40A100N6 is a 2 lines Common mode filter with ESD protection for High Speed Serial interfacehttps://www.st.com/en/protections-and-emi-filters/ecmf2-40a100n6.htmlThe input is identified as D+ to connector and D- to connector. The outputs are ide...
Hi, I have two pin connection questions, related to EMIF03-SIM02M8: 1) Are VDD pins 1 & 8 connected internal to the chip or should be connected together externally?2) Pin 9, GND does it have to be connected to system ground, or that's optional?Any la...
Hi, I hope you can help me. I'm working with STNRG012 on a power supply. we have already done the prototype, how ever we can make it run due to that STNRG012 needs a programming device (STEVAL-PCC020V2). This device is active but out of stock and I c...
Can i know the minimum Operating temperature of this IC "STTH112A-TR"will it support negative temperature "-40"
I saw somewhere in the forum that the TOF sensors see [optical] pings from other sensors as ambient light (meaning they are able to ignore them) but are still able to detect their own bounce. Is that true? If yes, can someone explain how that works...