SD1731-11
Does anyone here have a datasheet for part# SD1731-11? I see on website only datasheet SD1731 and SD1731-14. Does anyone know what the "dash #" stands for?
Does anyone here have a datasheet for part# SD1731-11? I see on website only datasheet SD1731 and SD1731-14. Does anyone know what the "dash #" stands for?
I am looking for the component number marked EVU T03 GP442 casing SMB.Thank you
Dear Support, Please advise the difference between part numbers STL23NM60ND1311 and STL23NM60ND. Verify their interchangeability as well. Can be replacements for each other. Thanks
ST M29W640FT 70N6H flash Nor chip with 20 erase write stored in temperature 33-36C and no powered In this case, what is the most approximate and realistic estimate of years for it to retain all the information written on this chip? an approximate num...
Hi everyone,I am trying to establish communication between the L9663 and an airbag sensor using PSI5. However, the behavior I observe on the oscilloscope is shown in the picture, with ramps instead of clear pulses. Since PSI5 uses the same wire to se...
NOR flash memory chips behave the same as other types of flash memory. If I energize NOR flash once a year, will it prevent any data loss? The datasheet says retention 20 years. If I energize it after 19 years, will it prolong data retention?in my ca...
Is this available anywhere? This is the Mahindra Scorpio Car BCM chip
Hello, This component, EMIF02-USB03F2, is listed as EOL. Do you have a direct/indirect replacement?Thanks,
We want burn LINUX image to NAND flash locatted? We follow the guidence of STMC2. But what should we do next? We can't find any guidence for next step.
my post is more formal than technical. Is it okay to use products that are based on GigaDevice microcontrollers? Is this company just competition, or does it violate ST patents and products with these chips should not be supported? What is ST's posit...