Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58x Cores Handling

Posted on January 10, 2018 at 13:24 Hello support Team, I am using SPC58x(Chorus 4M) uC. My Application SW running with Core2(Reset core). I want to check whether other cores in uC(like Core1,HSM core)working fine or not? can you suggest some method...

R PV by Associate II
  • 571 Views
  • 2 replies
  • 0 kudos

Resolved! Processor is in unknown state!

Posted on January 08, 2018 at 16:10hello everybody,we use the SPC56EL70 discovery board with Spc5 studio as IDE and UDE STK - 4.8 as Debugger.Today we got the following failure message - please see the following picture.The only thing we changed was...

0690X00000609O6QAI.png

SPC570S EEPROM Emulation, unable to write data

Posted on December 04, 2017 at 15:10Hello,I'm working with SPC570S-DISP discovery kit and SPC5Studio v5.6, and I'm trying to use EEPROM emulation in order to save some data for my application.I'm not using the flash drivers downloadable from ST site...

unhandled exception

Posted on December 21, 2017 at 14:42i am developing boot loader for spc56ec64l7 controller.my bootloader application is at address 0x00 and boot loadable application is from 0x0001_0000. i integrate flash driver from one demo project.when i try to u...

karan by Associate III
  • 688 Views
  • 1 replies
  • 0 kudos

SPC560B64L7 FlexCAN bootloader

Posted on December 18, 2017 at 04:05Hi, I'm currently using a SPC560B64L7 and I wish to go into bootloader via FlexCAN without connecting pin PA[8] and PA[9], is this possible to do so? Best if I could do all this in my application code.

Poon Jon by Associate
  • 508 Views
  • 1 replies
  • 0 kudos

Resolved! Connection between SPC5 Connect and SPC560B64L7

Posted on December 13, 2017 at 10:59Hello, if i wanted to program the MCU using SPC5 Connect via CAN, what kind of connection did I need to make between SPC5 Connect and the MCU? The MCU I currently using is SPC560B64L7.

Wong JS by Associate II
  • 1067 Views
  • 5 replies
  • 0 kudos

Resolved! How to use SD2 for Serial read/write on SPC570S-DISP

Posted on December 12, 2017 at 02:55Hi,I am using sample application for serial operation on SPC570S-DISP, from serial_lld.c, it looks like SD1 is mapped to LINFLEX0 and SD2 is mapped to LINFLEX1. I have no problem read/write SD1, however i need at ...

Job Shen by Associate III
  • 1297 Views
  • 4 replies
  • 0 kudos