2017-12-17 7:05 PM
Hi, I'm currently using a SPC560B64L7 and I wish to go into bootloader via FlexCAN without connecting pin PA[8] and PA[9], is this possible to do so? Best if I could do all this in my application code.
2017-12-19 1:08 AM
Hello Poon Jon ,
on SPC56, to use the bootloader via FlexCan, you should enable ABS and FAB.
FAB and ABS pins is implemented on SPC56 family
on SPC57,SPC58 ,the internal signals, which were originally driven by those pins, is tied to ´0´.
I think that you should create your own bootloader.
Anyway , I will check with experts.
Best regards
Erwan