2017-12-11 5:47 PM
Hi,
I am using the sample application SPC570Sxx_RLA FreeRTOS SERIAL Test Application for Discovery and my hardware is the SPC570S-DISP board.
I found that if i enable the 'Use software timers' in the SPC5 FreeRTOS component RLA, then generate and build the code, and program the board, debug through it, it suppose to stay in the 'vTaskStartScheduler();', but it doen't. It will step through it and fail the sample application. I wonder what is the cause for the failure? According to FreeRTOS documentation, if it run out of heap or other problem, it will step out of the vTaskStartScheduler().
Did i do something wrong or the software timer is not supported?
BTW, i noticed the Timer task stack depth is 2048, is that too much? I sort of noticed that during my experiment of my application, if i asked for 1000 stack depth for my task, the application will fail. But for the timer task stack depth, the range is 1024 - 8192.
Best Regards,
Job
#spc570s-disp #soft-timer #freertosSolved! Go to Solution.
2017-12-14 3:53 AM
Hi Job,
sorry for the issue. Let me explain the root cause: when you enable the software timers, a further task (timer task) is created. The stack size of this task is specified through the configuration parameter 'Timer task stack depth', set by default to 2048. This value is NOT the size in bytes. The size in bytes is calculated as (2048 * sizeof( StackType_t )), where StackType_t for our platforms is 4bytes. So, in other words, the stack size for the software timer task is, by default, 8k. Moreover, in our test application other 3 tasks (vTaskOne, vTaskTwo and the idle task) are created. For these tasks the stack size is (configMINIMAL_STACK_SIZE * sizeof( StackType_t )) = (256 * 4) = 1k. So, overall, to work fine our test application with the software timer enabled requires at least 11k. But in our test app the heap size for FreeRTOS is set to 8k. For this reason the test app fails when the software timer is enabled. In order to solve the issue, you can increase the heap size (for example, from 8192 to 12288) or reduce the software timer stack size (for example, from 2048 to 1024, that means 4k). Last but not least, please let me underline that in the heap and stacks dimensioning it is better to guarantee a small margin because a small part of memory is used to manage the control structures.
Best Regards,
Lugi
2017-12-12 12:49 AM
Hello Job ,
I have requested some helps from the application team.
Best Regards
Erwan
2017-12-13 1:54 AM
Hello Job ,
the recommandation for a software timer is to use 2048 as a limit of your task size. (it is an example)
Anyway , if you set 1024, it seems to work. I have no problem in the software timer (Task Priority 3, Timer Queue Length 10)
in FreeRTOS point of view,
the minimal Stack size is 256.
for your task (Size 1000) , you have maybe :
Best Regards
Erwan
2017-12-13 12:01 PM
Hi Erwan,
Thank you very much for trying it out.
For the SPC570Sxx RLA FreeRTOS SERIAL Test Application for Discovery sample application, if only change the Timer task stack depth to 1024, it will work. I tried different value and found that stack depth 1125 will fail and 1120 will pass. (i didn't need to narrow down further). The sample application created 2 other tasks which use stack size 256.
Then i tried with our application which has 3 tasks each set to stack size 256, and if i enable timer with 1024 timer stack depth, it will fail. I had to comment out one task in order to make the application run.
This comes to a conclusion that if want to use freeRTOS software timer, your application is limit to 2 tasks with 256 as stack size, and timer stack depth set to the minimum 1024 (or 1120 if you need some extra byte for the stack).
Could you confirm this conclusion is correct? Or there is a global configuraion somewhere which can increase the default overall stack cap to allow more tasks to be created.
Best Regards,
Job
2017-12-14 3:53 AM
Hi Job,
sorry for the issue. Let me explain the root cause: when you enable the software timers, a further task (timer task) is created. The stack size of this task is specified through the configuration parameter 'Timer task stack depth', set by default to 2048. This value is NOT the size in bytes. The size in bytes is calculated as (2048 * sizeof( StackType_t )), where StackType_t for our platforms is 4bytes. So, in other words, the stack size for the software timer task is, by default, 8k. Moreover, in our test application other 3 tasks (vTaskOne, vTaskTwo and the idle task) are created. For these tasks the stack size is (configMINIMAL_STACK_SIZE * sizeof( StackType_t )) = (256 * 4) = 1k. So, overall, to work fine our test application with the software timer enabled requires at least 11k. But in our test app the heap size for FreeRTOS is set to 8k. For this reason the test app fails when the software timer is enabled. In order to solve the issue, you can increase the heap size (for example, from 8192 to 12288) or reduce the software timer stack size (for example, from 2048 to 1024, that means 4k). Last but not least, please let me underline that in the heap and stacks dimensioning it is better to guarantee a small margin because a small part of memory is used to manage the control structures.
Best Regards,
Lugi
2017-12-14 11:45 AM
Hi Lugi,
Thank you for your detailed answer, it cleared my doubts perfectly.
I forgot there is always an idle task there which uses 256 words memory (1KB). In the application SPC5 FreeRTOS Component RLA, there is configuration for minimum Task stack size set to 256, i suppose it can be reduced if there is such needs. But i don't know where is the configuration for heap size for freeRTOS (8KB), could you point out?
The SPC570S-DISP has 512KB code and 32KB data of flash memory, also 48KB SRAM, i wonder where are are the memory allocated? Is it from the 32KB data flash memory?
Best Regards,
Job
2017-12-15 12:06 AM
2017-12-15 5:12 PM
Hi Luigi,
Thank you very much.
I increased the Total heap size for freeRTOS from 8192B to 11264B and reduced software timer task stack depth from 2048 to 1024 (words), now my application works fine. I have 4 tasks plus idle task (1KB stack memory each) and one periodic timer.
I found 10240B heap for freeRTOS doesn't work for my application, though i calculated freeRTOS memory usage by my application
- software timer 4KB
- 4 tasks plus idle task, 5 x 1K = 5KB
- 2 queues each 400B, total 2 x 400 = 800B
total is a bit less than 10240B, anyway 10240B failed and 11264B worked.
Best Regards,
Job
2017-12-18 12:03 AM
Hi Job,
I'm glad to know that now your application work fine. As I explained before, it is necessary to configure the heap size a little bit more than the sum of the memory used by all the tasks involved in your application because a part of the memory is used to manage the OS control structures.
Best Regards,
Luigi