Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPC58EC I2C signals not output at all

Posted on September 18, 2017 at 13:13HelloI am trying to implement a I2C driver on a SPC58EC.The problem I am facing now is that I cannot get the signal output on the pads correctly.IBSR.IBAL is immediately set when I try to generate a START conditi...

Resolved! Failed write the IIC register ICBR of SPC584C70E3FMC

After IIC module is initialized, when I prepared the data and to write the IBCR register to send it, after the register is written with the value 0x70(master mode, tx mode, interrupt enable and generate START condition), the value read from the IBCR ...

0693W00000YAPjbQAH.png 0693W00000YAPjlQAH.png
JJaso.1 by Associate
  • 518 Views
  • 2 replies
  • 0 kudos

SPC5 I2C driver

Posted on May 06, 2016 at 15:02Hi all,I'm currently working on a project where I need I2C communication between a SPC560C and an RTC. I'm using SPC5 studio for this, and when I go to ''SPC560BCxx Low Lever Drivers Components RLA'' there is a checkma...

mitchel by Associate II
  • 397 Views
  • 1 replies
  • 0 kudos