Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58 - Finding the IRQ number when handling IVOR04

Hello ST Community,Does anyone know which register I can read to find which IRQ triggered an IVOR04 exception, on SPC58?I am using the software vector mode, and the interrupt controller (INTC_IACKR) only gives me the address of the ISR... which is un...

FCasa.9 by Associate
  • 1495 Views
  • 1 replies
  • 1 kudos

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/SPC58xHxx, Advanced GTM and USBTypeC credentials should be requested on credentials@spc5studio.comNew or updated componentsRLA 1.9.0...

Resolved! PIT timer of SPC560P50L5 to be used for wake up

We use SPC560P50L5 in an automotive-qualified battery management system for starter batteries. PIT timer of this device should be able to generate a wake-up interrupt when in low-power mode.At this moment, PIT timer 3 is already working to generate a...

Resolved! Code wait and stay alway.

Hi,The demo I use is SPC560BCxx_RLA CAN Test ApplicaiontDebug LOOP Mode is OK.In Normal Mode, when I use can_lld_transmit to send CAN messages, the status returned is always CAN_MSG_WAIT. Can you help me analyze this problem?A preliminary confirmatio...

0690X000008wTdOQAU.png 0690X000008wTd4QAE.png 0690X000008wTdTQAU.png

Resolved! Is it possible to disable 8x division for system clock?

Hello,I am bringing up an SPC570S50E1. Using the dev kit I am able to successfully bring up and run some simple code, but I observe a clock division for the clock going into the core.When I route out clockout with a divider of zero and sysclk running...

AZayt.5 by Associate II
  • 1679 Views
  • 2 replies
  • 0 kudos

Resolved! How to enable “Divide by Zero�? exception for SPC56EL60

1)    Could you please tell how to enable “Divide by Zero�? exception for SPC56EL60 controller ?2)    What happens if exception is not enabled, what is the behavior of controller ?NOTE: This question and answer originated from a customer support case...