Resolved! I would like to know about the SARADC Test Application code.
I need help understanding the SARADC test application code. Can anyone explain to me how the code works?
I need help understanding the SARADC test application code. Can anyone explain to me how the code works?
I tried to initialize test channels on SARADC_B (supervisor)./* Channels Configurations (DMA is not used)*/ static channelConfig _saradcconf_ch_configs[SPC5_SARADC_MAX_NUMOFCHANNELS] = { {SARADC_CHANNEL_TEST, 96U,SARADC_REFERENCE_DEFAULT, SARADC_PR...
On the SPC582B, there is only one SARADC and I would like to reduce the SW time needed for ADC conversion.I have about 15 ADC to convert and they are not contiguous.I use the SARADC in scan mode and I would like to retreive my ADC data in a buffer in...
I tried to change the chanel number but it didn't work, and i also tried to change the driver under test but it gives me an error. here is my void mainhere is the pin map
My question is how to set the sample rate exactly? I know that I have to set it via the CTR register and there via the values INPCMP and INPSAMP. I also know where to set the values in the LLD-Config. However, I do not understand which change of the ...
I tried setting up with default configuration parameters for ADC 1 on the SPC560PXX. However, it provides some random values. In the conversion timing register, I verified that INPSAMPLE's SPC560PXX default value is 5. When creating a Conversion grou...
Hi, i want to ask regarding the sensor library. As i new to SPC5Studio, i want to connect the displacement sensor. So , do i need to declare the sensor library as a header or just simply can use the ADC header library?
I want to use the PE7 pin of SPC560B to detect analog quantityThis requires reusing it as an ADC input pinHow should I configure him?
Hello,In the SPC5Studio, eDMA comes enable defaultly. My question when I enable ADC Module, conversion of analog channel is done through eDMA ? If not should I need doing some configurations ?Best Regards,
Posted on October 11, 2017 at 11:54Main target is to send an ADC-value to the CAN-BUS.I took the SPC570xx_RLA CAN Test Application for DiscoveryModified Pin Settings:in main.c I tried to initialize and use the ADC:Without ADC-code CAN example works ...