StellarStudio using Jlink Debug issue
Hi, I using the GDB SEGGER J-link with JTAG debug, and stuck in "Setting breakpoint @ address 0x24001362, Kind = 2, Type = THUMB, BPHandle = 0x0001Starting target CPU..." Please help, thanks~
Hi, I using the GDB SEGGER J-link with JTAG debug, and stuck in "Setting breakpoint @ address 0x24001362, Kind = 2, Type = THUMB, BPHandle = 0x0001Starting target CPU..." Please help, thanks~
Hello, Stellarstudio how to set the code optimization? During the process of compiling a.C file into an.O file, the code is optimized. Commonly used optimizations include time optimization, which aims to make the code execution time shorter and more...
We are using SPC58xNx 32-bit Power Architecture microcontroller for automotive ASILD applications.We are using third party flashing tool to flash data section multiple time. We are able to flash hex file 12-15 times successfully. But random time it m...
I would like to know that, what are the minimum DCF configuration required to activate the HSM core in Stellar SR6G7? Is there any Lauterbach cmm script available to flash the UTEST DCF configuration?
Hello,I am trying to run Projects\System\SIUL2\siul2LedBlink from StellarSDK_4.0.0 on a SR6G7EVBC4000P_RevA board. The project was successfully build. To flash the board in RAM, I am using the last version of Lauterbach. When running, it seems that i...
For your information , StellarStudio 6.0.0-IRON version is officially pushed (for SR5x & SR6x). (Windows, Macos, Linux) based on eclipse 202309 and the version CDT 202309 with its standalone tools https://www.st.com/en/development-tools/stellarstudio...
hello, I had read the "um3201-getting-started-with-stellar-studio-ai-plugin-for-artificial-intelligence-ai-stmicroelectronics" document, where can I find the AI Editor software to be launched like in page 5 ?Best regards, Laurent
Hi,I've just gotten a new microcontroller SPC58EC-DIS from elfa. From my past I worked a lot with STM so I wanted to try something new, but this was the first time that I got something like this:Is it normal that the board comes with soldered wire be...
Stellar SR6 G7 line : Where can get SR6G7C6 Steller Need Technical reference manual please
hi i am new to the controller, i read the manual that dcf records contains the configurations like if device boots up it performs some basic tests and then basis on the application address provided in dcf record, it jumps to application, but that add...