Skip to main content
karan
Associate III
December 21, 2017
Question

unhandled exception

  • December 21, 2017
  • 1 reply
  • 1045 views
Posted on December 21, 2017 at 14:42

i am developing boot loader for spc56ec64l7 controller.my bootloader application is at address 0x00 and boot loadable application is from 0x0001_0000. i integrate flash driver from one demo project.when i try to use pFlashErase() its stuck in unhandled exception.i think boot ladable application page is erased but code stuck in 

unhandled exception.here i attach screen shot of cpu resister which shows that it goes in unhandled exception from pFlashErase()  and also attach project.can any one help?

#flash-erase #spc56-flash
This topic has been closed for replies.

1 reply

Erwan YVIN
ST Technical Moderator
December 22, 2017
Posted on December 22, 2017 at 09:34

Hello Patel ,

you should check your PC (Program Counter) and LR (Link register) to investigate where the issue is coming.

i will ask some flash experts.

          Best regards

                        Erwan

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.