Resolved! Hi, I'm evaluating a solution for a 1 ms reading using the SDADC driver provided with the SPC Studio (SPC58NE). I found this check in the code, that sometimes causes a missing reading. I add a comment with the SFR register that I'm currently using.
uint8_t sdadc_lld_read(SDADCDriver *sdadcp, float* converted_value) { int16_t data; uint8_t return_value = SDADC_DATA_NOTVALID; /* check if valid data is available */ if (sdadcp->sdadc->SFR.B.DFEF == 0U) /* <- Check if the FIFO is not emp...