2025-01-22 5:49 AM
Hi
I try to program SPC564B74L7 target with using BAM function by serial port (SCI). I use an FTDI USB to RS232 adapter (USB-RS232-WE-1800-BT-0.0). Despite several attempts, I can't connect to the target from SPC5FlashProgrammer (version 2.8.1 Beta). In the Interface drop-down menu, I have selected my UCUART::FTDI/0/UART cable (which is the only suggestion). I have no activity on the serial bus when I click on Connect. Has anyone encountered the same problem as me and would they have a solution?