Does SPC58EC80E5FMCOX supports CAN overload error?
Hi Team,Do you know SPC58EC80E5FMCOX supports CAN overload error or not?Best Regards,Abhishek
Hi Team,Do you know SPC58EC80E5FMCOX supports CAN overload error or not?Best Regards,Abhishek
Hi Team,I am working on SPC58NE84.Does SPC58NE84 supports CAN overload error? Best regards,Abhishek
Currently I am making a can gateway system.After receiving the data through can interrupt, task send data periodically.The problem is that sometimes strange values are sent when sending.For example, a value of 10 was being received, but other va...
Problem: Acknowledgement error on can analyzerWe are able to get the transmit data on TxFIFO Registers for CAN channel 2 but hardware is unable to transmit the message on the CAN channel 2.May I know what we can do to correct this problem asap? #[ST...
Please answer..
Does the SPC560 can program in appilication (IAP) ?How CAN I do to implement the user bootloader? Is there any document about it? and the Chip has the BAM, is it means that ,I can user the factory bootloader to update the program via usart or FlexCan...
I´m using the l9616-tr CAN transceiver, but i have no signal of CAN comuniccation, i think maybe tx and rx configurations pins are inverted.
Hi. I use the spc58nh-disp board.I'm doing the CANFD gateway test.I uses CAN0 and CAN1.After receiving 55(id quantity) rx message from CAN1, CAN0 Transmits 55 messages.And after receiving one message from CAN0. Transmit to CAN1.At this time, bus...
I am trying to set the CAN bus rx filter so that only the CAN message IDs that I specify in the can_lld_cfg.c file will be received. I tried to use the CAN classic filter setup for extended IDs. I set the mask to all ones (0x0fFFFFFFUL) so, it should...
Hello ,I am facing an issue wherein the CAN transmit message is sending wrong data for one sample in between the transmission. Please see the below screenshot.T3_C1_ECU_SCIMO_PE_CTRL_MOT is a transmit frame with a cycle time of 10ms. The transmission...