Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! spc56x series bootloader

Does the SPC560 can program in appilication (IAP) ?How CAN I do to implement the user bootloader? Is there any document about it? and the Chip has the BAM, is it means that ,I can user the factory bootloader to update the program via usart or FlexCan...

XDB.1 by Associate
  • 530 Views
  • 1 replies
  • 0 kudos

SPC582B - writing boot-loader to be used with BAF

I would like to write a simple boot loader to be uploaded to SPC58's RAM by BAF (according to "Boot Assist Flash" section of RM).The boot loader's job is to receive the program by LinFlex or CAN and store to MCU's flash. All this without need of usin...

Yannek by Associate III
  • 1134 Views
  • 5 replies
  • 0 kudos

Resolved! Bootloader example code for SPC560P50L3 controller

Hi All,I'm searching for example Bootloader code for SPC560P50L3 controller ( 100 pins package). I tried import from the example code in SPC5 studio, but it is for a SPC560P50L5 controller. How I can convert this code SPC560P50L35controller ( 144...

SPC560P40 series Bootloader

I want to develop a bootloader for SPC560p40l3 controller.I've read about BAM and SBL.But that method is Hardware dependent, i.e we've to give 1 logic to a[4] to get it into boot mode(CAN/UART).I don't want to use the internal Boot module.Is there an...

Aakash by Associate
  • 406 Views
  • 1 replies
  • 0 kudos