User Activity

Posted on December 12, 2017 at 02:55Hi,I am using sample application for serial operation on SPC570S-DISP, from serial_lld.c, it looks like SD1 is mapped to LINFLEX0 and SD2 is mapped to LINFLEX1. I have no problem read/write SD1, however i need at ...
Posted on December 12, 2017 at 02:47Hi,I am using the sample application SPC570Sxx_RLA FreeRTOS SERIAL Test Application for Discovery and my hardware is the SPC570S-DISP board.I found that if i enable the 'Use software timers' in the SPC5 FreeRTOS c...
Posted on November 30, 2017 at 02:49Hi,I need to use UART to send data from the SPC570S-DISP to a different board, looking at the UM2025 User Manual for the SPC570S-DISP: Discovery + Evaluation Board, section 2.9 LINFlex and UART, it says the LINFle...
Posted on November 29, 2017 at 02:34Hi,We have the SPC570S-DISP board which has the SPC570S50E1 MCU. The SPC5Studio Import application Wizard only has SPC570S50L1DISP for the SPC57 S-Line.After import application such as SPC570Sxx_RLA SERIAL Test Ap...
Posted on November 23, 2017 at 00:43Hi,I have the SPC570S-DISP Evalution board which connect to my Windows 7 deskstop. Following the instructions from the ''PLS Debugger Installation driver on SPC560X Discovery board'' comes in the SPC5Studio softwa...