Hi everybody. I am using "STM32H7B3LIHQ" MCU and i want to try led blinking. I have created a new project in CubeMx. I am using 24MHz crystal resonator and MCU frequency is 280 MHz. &nb...
Hello, I use STM32F767ZI (on a board NUCLEO-F767ZI) , CubeIDE, HAL driver and I try to communicate with an accelerometer (LIS2DW12 on the board SEN0405) with SPI interface. I'll try to give the more...
Hi All! I'm doing a project on the STM32F429 discovery board. In this project, I've used the TouchGFX. Also, I'm using the FreeRTOS. The idea is to read the Temperature sensors and read their valu...
I am experiencing issues with the VBAT pin on the STM32H563ZIT6 microcontroller. Specifically, the VBAT pin is not responding properly. I am using a CR2032 CMOS battery for RTC backup, but it is not ...
Hello, I am trying to find available solutions for below requirement. I am using STM32H743 MCU in a design and I want to add external SRAM of 128Mbytes to the design. I understand can do this...
Hi, We want to use now the STM32H5 for future projects. In the past, we used STM32F4 with enabled SWO for debugging. Is there any example available to get this feature working for STM32H503?...
I’m using an STM32G473 and I have TIM20 CHANNEL1 configured in output compare mode. When the compare value is reached, I want to move CNT values from TIM1, TIM5, TIM6, TIM7 and TIM15 to 5 static loca...
STM32F303 - Application running fine in CubeIDE debugger, custom board. It will not start as standalone, programmed with CubeIDE or CubeProgrammer with .elf or .hex. I have created an 'attach' run d...
Hi, The ADC test has only 2 channels: Vrefint and TempSensor. The following ADC result (convertedData) is read out through DMA: tick = 1s - convertedData[0] = 113968573 convertedData[1] = 0
tick ...
Hello, I've started to develop with the Riverdi STM32 Embedded Display and I'm trying to use the CAN BUS to display data, but unfortunately I can't. I'm not receiving any data. The CAN on the board ...