STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bring up the STM32MP135x - Share Training Course (I)

Take MYIR’s MYD-YF13X and the STM32MP135F-DK as examples to share training course on how to use STM32CubeMX combined with the developer package to implement the booting of the minimal system.https://www.myirtech.com/news_list.asp?id=8771. Development...

stcourse001.jpg stcourse02.png stcourse03.png stcourse04.png
LZhan.22 by Associate II
  • 1460 Views
  • 2 replies
  • 2 kudos

Resolved! STM32MP15 ECO 5.0.0 OPTEE Panic set_clock_then_voltage

On STM32MP1 discrete power.  512MB DDR , TF-A & OPTEE configure in SYSRAME/TC:0 0 Panic at core/arch/arm/plat-stm32mp1/cpu_opp.c:106 <set_clock_then_voltage>Log attached.This message seems to unique for stm32mp1 in OP-TEE  code. no other platform sou...

debugging_0-1694760334568.png debugging_0-1694770056411.png debugging_0-1694776876106.png

We have developed a custom board using STM32MP157AD3 chipset and STPMIC. We did develop a dts using CubeMX and did all the patches as mentioned in Lab documentation. But we came accross 2 errors.

When we use the PMIC values from DK2 example.1 . ERROR:  regul ldo3: max value 750 is invalidWARNING: register_pmic:600 failed to register ldo3PANIC at PC : 0x2fff05cb2 Next we tried setting the ldo3 max, min values to 3V and 1.8V and it was working ...

NP by Associate II
  • 5936 Views
  • 11 replies
  • 0 kudos

Resolved! STM32MP135F-DK How to set LDO2

Hi, I have an STM32MP135F-DK board, and I want to set LDO2 and get an output voltage of 3.3V. I have read a document ( Integration of STM32MP13x MPU product lines and STPMIC1D / STPMIC1A on a wall adapter supply) which states that LDO2 must be set af...

gunesalp by Associate
  • 2186 Views
  • 1 replies
  • 0 kudos

STM32MP151CAA3T length matching

My question is what the recommended values are for STM32MP151CAA3T (see image for Altium xsignals creation for the routing).I am currently doing routing and I could not find all this information in the datasheet. 

Drive DSI data lanes to LP-11

Hello. I need to integrate a TI SN65DSI83 bridge with a DK2 board and one of the requirements of that bridge is to drive the data lanes to LP-11 state. What is the procedure to make that happen? I am assuming I need to make changes to dw-mipi-dsi / d...

EMaes.1 by Associate II
  • 1128 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP135 PANIC and DDR frequency error

Hello ST community,I am designing a board with STM32MP135 CPU and DDR3L based from STM32MP135F-DK.DDR stress test passed successfully and tf-a files are adjusted to have I2C4 on pins used in my design (SCL on PB13 and SDA on PB7).When I flash board t...

Vince60_0-1694011522130.png Vince60_1-1694011539770.png
Vince60 by Associate II
  • 3571 Views
  • 4 replies
  • 1 kudos

Enabling the GPU on a DPI panel

Hi, I have a custom board with a parallel RGB display connected to it that works OK when using pixman.If I enable the galcore.ko module, weston fails;  [15:27:38.101] weston 10.0.0 https://wayland.freedesktop.org Bug reports to: https://gitlab.freede...