STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! browser support on STM32MP25

Hi, I am currently working on a project that requires us to install a browser on our board. We are using an STM32mp25, which is using the Mickledore image. I am finding that the meta-browser layer is not compatible with Mickledore, and if I'm not mis...

Size of the file read by ROM code

Hello,I am developing on the STM32MP131FAE board in a bare-metal environment.This chip does not have internal Flash, so I am planning to load a bin file from external Flash at initial boot.The Flash will store two bootloaders and two main firmware im...

Stnoobs by Associate II
  • 192 Views
  • 0 replies
  • 0 kudos

how to access the adc and dac in stm32mp157d-dk1

i am using stm32mp157d-dk1 and i am using virtual box and i want to make a gui using c++which application should i use so that i can access the adc and dac in linux.using arm cotrex a7 can i access/control the adc and dac. for example when I click a ...

Sharan by Senior
  • 484 Views
  • 6 replies
  • 2 kudos

Resolved! Can STM32MP151 transfer sound via HDMI connector?

I'm buildning my own computer by using STM32MP151AAC3.I'm going to draw lines for the HDMI connector. I have one question: Can I transfer sound via the HDMI cable? For example if I run OpenSTLinux onto the STM32MP151AAC3 processor, and then I connect...

DMårt by Lead
  • 1237 Views
  • 12 replies
  • 0 kudos

USB device function problem on MP135

Hi all,I'm writing a USB composite device support (baremetal) for MP135: it must support a custom interface and a CDC profile. Now I'm testing the CDC side connecting the USB cable with a PC: Windows mounts correctly a virtual serial port and I open ...

SteMMo by Associate III
  • 177 Views
  • 1 replies
  • 0 kudos

IWDG1 bit is not set in RCC status register

Hello     We are using STM32MP157A processor in our custom board.      Now we are implemented IWDG1 in Cortex A7 processor. The IWDG1 bit is not going to set after reset the processor with Watchdog timeout.we checked in following registers• RCC BOOTR...