STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debugging M4 with GDB from command line?

I would like to understand what the Eclipse IDE is doing to start the debugger, so that I can move away from using it. I much prefer CMake and other tools. I'd be grateful for any assistance. The wiki section for this is TBD.I'm not too familiar with...

unicycle by Associate III
  • 1911 Views
  • 6 replies
  • 0 kudos

Resolved! Maximum 4 virtual uarts can be created?

Hi,As i was testing the limit of how many virtual uarts i can create, i found that the limit is actually 4:Using debug tracing i can see that the channels get created inside the code (here i am creating 5 virtual uart) but only 4 ttyRPMSG are created...

0690X000009ZdF8QAK.png
victor.b by Associate II
  • 506 Views
  • 1 replies
  • 0 kudos

Could not debug the OpenAMP_TTY_echo

Hi,I am following the tutorial of developing on M4 with the STM32MP1 but when I do the"debug as" to this project, it comes out an error.The STM32MP1 has connected to my PC through the STLINK usb; the boot0 and boot2 on the board have been set to "on"...

0690X000009ZaoFQAS.png
DXu by Associate II
  • 1206 Views
  • 2 replies
  • 0 kudos