STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Linux image for a qt based app

Hi there STM team!I need to build a embedded Linux image for a STM32MP15 target. My application has a QT GUI already implemented. What is the best approach to create this image? I know OpenSTLinux exist but I don't fully understand what's the advanta...

JPabl.1 by Senior
  • 207 Views
  • 1 replies
  • 1 kudos

No interrupt generated on USB Host for STM32MP135F-DK

Hi all,I'm trying to enable the host functionalities for USB Port1 for MP135: I imported the Host Library and implemented some functions on usbh_conf.c file. Attached to the DK board I have a optic mouse.After some basic initialization I'm in the USB...

SteMMo by Associate III
  • 213 Views
  • 3 replies
  • 0 kudos

build image

after following the bellow steps and in build-<distro>-<machine>/tmp-glibc/deploy/images/<machine> directoryi cant find the file system image(FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv) in this directory as i am using stm32mp157d-dk1 and it contain...

Charan28 by Associate
  • 174 Views
  • 1 replies
  • 0 kudos

Disabling TEE firmware

The following output seems to be the default: root@stm32mp2:~# cat /sys/class/remoteproc/remoteproc0/fw_format TEE  However, for debugging purposes, I would like to turn off firmware verification, and make the remoteproc driver accept plain ELF files...

manuelW by Associate
  • 142 Views
  • 1 replies
  • 1 kudos

RAM for STMP157

Hi,I am building my STMP157 board using the reference of "STMP15X-SOM" of Olimex. In that the RAM used is K4B4G1646D-BYK0, but I am unable to find the part number in online store. Can you please help me in finding the different RAM which can be used ...

muffss by Associate II
  • 312 Views
  • 5 replies
  • 0 kudos

STM32MP135F custom project with no I2C bus

Hello. I am trying to get a custom design using STM32MP135F to boot.Unlike the DK, it does not use I2C busses, and I2C is not listed in the DTS files as created by STM32CubeMX.I follow the wiki "How to compile the device tree with developer package" ...

Resolved! Getting lost when installing dristibution package

I'm trying to install the distribution package but I'm at the point of the proxy issues and I don't know what to do.  sudo apt-get update sudo apt-get install corkscrew git config --replace-all --global core.gitproxy "$HOME/bin/git-proxy.sh" git con...

JPabl.1 by Senior
  • 400 Views
  • 2 replies
  • 0 kudos

Why my computer can't ping STM32MP135F-DK?

The Static IP settings of my computer are as follows As follows, My computer can ping itself Then the Static IP (/lib/systemd/network/52-static.network) of my STM32MP135F-DK is set as follows As follows, My STM32MP135F-DK also can ping itself Why...

syuan_0-1730519185369.png syuan_1-1730519342431.png syuan_2-1730519678133.png syuan_3-1730519730430.png
syuan by Associate
  • 259 Views
  • 1 replies
  • 0 kudos

Resolved! browser support on STM32MP25

Hi, I am currently working on a project that requires us to install a browser on our board. We are using an STM32mp25, which is using the Mickledore image. I am finding that the meta-browser layer is not compatible with Mickledore, and if I'm not mis...

Size of the file read by ROM code

Hello,I am developing on the STM32MP131FAE board in a bare-metal environment.This chip does not have internal Flash, so I am planning to load a bin file from external Flash at initial boot.The Flash will store two bootloaders and two main firmware im...

Stnoobs by Associate II
  • 191 Views
  • 0 replies
  • 0 kudos