STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I need a roadmap for a STM32MP157C-DK2 project

Hi,I am only a bit familiar with embedded linux. I will develop a demo project with STM32MP157C-DK2 with C language:on M4 side, a sensor(BME280) and a vantilator (5v) are connected. Sensor is to read periodically and three numerical values( temp, hum...

IYetk by Associate III
  • 585 Views
  • 1 replies
  • 0 kudos

4 questions about "st-example-image-qt"

Hello,I have 4 questions if you have time to answer, I would appreciate it very much.I prepared st-example-image-qt image. But there isnt any terminal like weston image. Should I run any other command before bitbake in order to have all the tools pac...

IYetk by Associate III
  • 689 Views
  • 4 replies
  • 0 kudos

Resolved! Could not queue DRM page flip on screen DSI1 (Permission denied)

HII've already run this command​Continue to run​root@stm32mp1:~# /usr/share/examples/opengl/hellowindow/hellowindowqt.qpa.input: X-less xkbcommon not available, not performing key mappingCould not queue DRM page flip on screen DSI1 (Device or resourc...

0690X000009YSI7QAO.png
User.44 by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

Resolved! Display in separate module

Lets say I need to separate module, one will contain the pcb with mpu and other IC, the second will contain a touchscreen display and sensors. The modules are 2 meters apart. What should I use hdmi or mipi? How do I send mipi over distance?

GEspi.19 by Associate
  • 448 Views
  • 1 replies
  • 0 kudos

Reliability of M4 and A7 through RPMSG

I wrote an application on the STM32MP157C-DK2, and m4 reads the data of an external adc and sends it to A7 for processing. The entire program got stuck after running for about 15 hours. The console has been outputting the following content[84306.5118...

Jzhua by Associate III
  • 717 Views
  • 4 replies
  • 0 kudos

stm32mp157C-DK2 development board test problem

The routine I tested was stm32mp157\STM32Cube_FW_MP1_V1.0.0\Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_TTY_echo, The test method is guided by the following address, https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP1...

Zonlo by Associate
  • 691 Views
  • 2 replies
  • 0 kudos

Imaging the provided SD Card

I'm trying to image the provided SD Card. I'm trying to use `dd` but it seems to only be cloning about 33mb before saying it is finished with no other output. sudo dd if=/dev/disk2 of=~/stmicro.imgAny thoughts?

JSlac by Associate II
  • 786 Views
  • 2 replies
  • 0 kudos

Resolved! Looking for ODB++ Data of STM32MP157C-DK2

I want to setup a Boundary Scan project for the Deveklopment kit to learn Boundary Scan with STM32MP157C. Therfore it is very helpful to use ODB++ data of the development kit.Can you provide this (maybe under NDA)?

W. Alex by Associate
  • 695 Views
  • 2 replies
  • 0 kudos