STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Secure SPI on STM32MP157-DK1

Hey everyone,I am working on STM32MP157-DK1 with trustzone cortex-A.I want to use SPI in secure side, but it's possible only with SPI6 that is not mapped to the outside.It's possible to activate SPI (1 ... 5) peripherals in secure side ? if not, why ...

simoBen47 by Associate III
  • 1165 Views
  • 4 replies
  • 0 kudos

Resolved! SMT32MP1 MCU as Power Management Unit

Hello.I want to use MCU (Cortex M4 core) as PMU for MPU (Cortex A7 core).Is it possible to use it in this way?For this I need the following:It's better to start MCU firmware from another source (not SRAM) - from non-volatile memory. Is it possible?Sw...

alexey.b by Associate II
  • 823 Views
  • 1 replies
  • 0 kudos

Resolved! Engineering mode and CA7 secure state

In RM it is stated that in Engineering mode (BOOT pins at 3'b100) the MPU re-opens CA7 secure debug.I boot in that mode, then halt in openocd:stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints > halt stm32mp15x.cpu0 rev 5, partnum c07, arch f...

Resolved! linux performance

I just got my dk2 kit, played with it a little bit, but the performance is so bad. it takes a lot to boot ~30sec and after that it is unresponsive, you click something, then several seconds later something happens. Is this considered normal, or it is...

Resolved! OPTEE, trusted APPS

I'm interested in learning about TF-A, OPTEE, are some demos concerning these topics available?Is it possible to debug the CortexA core, through the embedded ST-LINK? I mean working solution, not in theory?What would be limitations debugging very ear...

Resolved! I need a roadmap for a STM32MP157C-DK2 project

Hi,I am only a bit familiar with embedded linux. I will develop a demo project with STM32MP157C-DK2 with C language:on M4 side, a sensor(BME280) and a vantilator (5v) are connected. Sensor is to read periodically and three numerical values( temp, hum...

IYetk by Associate III
  • 588 Views
  • 1 replies
  • 0 kudos

4 questions about "st-example-image-qt"

Hello,I have 4 questions if you have time to answer, I would appreciate it very much.I prepared st-example-image-qt image. But there isnt any terminal like weston image. Should I run any other command before bitbake in order to have all the tools pac...

IYetk by Associate III
  • 692 Views
  • 4 replies
  • 0 kudos