STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to create an UART interface in device tree

Hello,I would like to use the UART7 with A7 on the STM32MP157C-DK2 with the openstlinux-20-02-19 ecosystem. Therefore i tried to include/enable the UART interface in the device tree but it is not working correctly. I configured UART7 in the stm32mp15...

PSchw.16 by Associate II
  • 3753 Views
  • 6 replies
  • 0 kudos

How to compile device tree for board ODYSSEY-STM32MP157C on arm-ostl-linux-gnueabi/linux-stm32mp-5.4.31-r0

Hi,I'm using your wikihttps://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-A7/Modify,_rebuild_and_reload_the_Linux%C2%AE_kernelto add some device threes that belongs to a different board ...

Boot to v5.4-stm32mp-r1

Hello,has anyone successful booted linux  v5.4-stm32mp-r1 on the stm32mp157c-dk2 board?If so can you please provide me a working config?I am trying to switch from the 4.19 kernel to v5.4-stm32mp-r1 but the boards freezes after trying to load the kern...

Artem by Associate III
  • 1520 Views
  • 5 replies
  • 0 kudos

Hello, I have a question regarding ST marketing on the STM32MP1 devices. According to the page, it states "STM32MP1 users can now choose from several IDEs from leading vendors and enjoy free license"

Which IDEs can be used for free in order to download/debug my application in an asynchronous fashion as two cores are running the the same time. I have taken a look on some suppliers (Tools & Software), but it looks like that you need to pay a some m...

PBart.3 by Associate II
  • 2294 Views
  • 10 replies
  • 1 kudos

Power startup with discrete power supply

Dear All,According to AN5256 "discrete power supply hardware integration" the power source for VDD is turned off in case of crash to "reset" the hardware using the PWR_ONRST signal. At startup. At cold startup and immediately after a crash the power ...

PGE by Associate III
  • 427 Views
  • 2 replies
  • 0 kudos