User Activity

Hello,will there be updates to the gcnano-binaries?The latest version (6.4.3) seems to be broken.When trying to start the cog browser (wpewebkit based) it crashes on eglCreateWaylandBufferFromImageWL.After reverting to gcnano 6.4.1 it is working agai...
Hello,has anyone successful booted linux  v5.4-stm32mp-r1 on the stm32mp157c-dk2 board?If so can you please provide me a working config?I am trying to switch from the 4.19 kernel to v5.4-stm32mp-r1 but the boards freezes after trying to load the kern...
Hello,I have the stm32mp157c-dk2 board and have connected two CAN Bus transceivers to it.FDCAN1 is assigned to the A7 CPU and the FDCAN2 is assigned to the M4 CPU.Both transmitters are connected to the same CAN bus. There is also a 3rd device connect...
Kudos from