STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tamper pins

Is there any application note for tamper pins? Which one of the pins is the active tamper?

Oitsh.1 by Associate II
  • 726 Views
  • 2 replies
  • 0 kudos

video codec

I am developing an industrial tablet with only one task - to display and record videoIt should be ready to work in a few seconds after turning on (that's why I also think about using STM32H7)I need to show on the display 720p (ideally 1080p) 30 frame...

ltdc-simple panel- parallel DRM mode fail

Hi i have a ltdc tft display RGB parallel display connected to stm32mp15 series,unable t0 get drm link to DPI connector, the code flow is breaking at following files,using DISTRO              = "openstlinux-weston"i have no idea where to start to deb...

Ara.1 by Senior
  • 989 Views
  • 1 replies
  • 0 kudos

Failed to download system image

Our self-made board contains emmc and lpddr3 (1GB, 32bit). The error message when downloading the image is as the attachment. Use Uart to monitor during the download process to get the following information:NOTICE: CPU: STM32MP157AAC Rev.Z NOTICE: Mo...

YWu.2 by Associate II
  • 2183 Views
  • 8 replies
  • 0 kudos

Resolved! How to configure parallel lcd in linux and u-boot?

I have a generic parallel LCD screen. 24 bits RGB, vsync, hsync, pclk, data_enable, disp_on,..The examples I see on the wiki only shows the HDMI connection and DSI. How do you configure this for DPI?Is this a good start? (In the device tree)panel_bac...

STM32MP1 can be equal to raspberry pi 4 ?

we using  raspberry pi 4 to run Apache python , mysql an c kernal and it runs excellent om 4 Giga ram.we would like to move to stm32p1 , can it being compare and be replaceable ?

maor by Associate III
  • 1252 Views
  • 1 replies
  • 0 kudos

Using RAUC with openstlinux

We are using rauc to perform remote updates on your target devices.However, to create the rauc bundle, rauc uses a different image format than the ST image created.The default imagesource in rauc is:imgsource = "%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' %...

meiss.M by Associate III
  • 2194 Views
  • 7 replies
  • 0 kudos