I am not using OTG (Only host USB's) in the PCB I connected OTG_VBUS to GND. Is this problematic? I saw that it should be left open but not sure if it is connected internally
I want to use a SIP with ST32MP153 and it uses PC13 to PMIC wakeup, PC1 is used for MDC so I'm left with only PI8 so can't use active tamper.I sit possible to use Ethernet without MDC so I can use PC1 for active tamper with PI8?
Hi Patrick,I'm using the 257 pins package of the STM32MP153 with Ethernet.So PC1 is used for ETH_MDC.PI8 is not available because of the package.Does this means I can't use active tamper?Regards,Ofer