STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157C-DK2 Uart Boot

Is it possible to boot over UART on the STM32MP157C-DK2? I set the BOOT pins as following:BOOT0 - OFFBOOT1 - OFFI am using the FT232 UART-USB Adapter and have connected the following pins:UART GND - CN16 GNDUART VCC - CN16 3.3VUART TX - CN14 ARD_D1UA...

ANiko.3 by Associate II
  • 2709 Views
  • 14 replies
  • 0 kudos

Resolved! Modify STM32MP157A dev kit with STM32MP151C

Hello,No dev kit is available for STM32MP151x microprocessors, do you know if it is possible to replace the STM32MP157 chip by a STM32MP151 one on the STM32MP157A-DK1 ?I have read that STM32MP1 are pin to pin compatible, but I want to be sure and if ...

Complex Project idea on STM32MP1 DK2?

I am working on STM32MP1 DK2 as a Hobby Project, can anyone suggest me a complex project to get to a linux + RTOS based project developement. I want to get an hands on idea on RTOS + Linux project. I saw a video of Zephyr project with Intel which ran...

sanket47 by Associate II
  • 671 Views
  • 1 replies
  • 1 kudos

STLinux Ecosystem v2 boot chain problems.

We have a custom board based on the STM32MP157 series, and are trying to get the TF-A boot chain working.  We have downloaded and compiled the linux kernel, u-boot, and arm-trusted-firmware for the STLinux ecosystem v2.  We can boot to u-boot, and th...

Macdog by Associate III
  • 704 Views
  • 1 replies
  • 0 kudos

How to use the RTL8723BU in "Ecosystem V2.0.0"?

Hi All​​If you create a distribution with RTL8723BU enabled in the Linux kernel and boot, you will see the error message below.[  30.102790] usb 2-1.2: 1f8: ff ff ff ff ff ff ff ff[  30.106213] usb 2-1.2: RTL8723BU rev E (SMIC) 1T1R, TX queues 3, WiF...

Machilus by Associate III
  • 818 Views
  • 1 replies
  • 0 kudos

Resolved! Key format for secure boot

Hi, I'm trying to generate secure boot keys using native linux tools. I assumed the secureboot format would be documented, but all I found was links to STM32MP_KeyGen.I can use openssl to generate ECDSA keys, and also get publik keys out. I am at teh...

mrnuke by Associate II
  • 695 Views
  • 1 replies
  • 0 kudos

Resolved! No wlan0 on DK1 I just received.

I have a pair of DK1 boards I just received that I wanted to get working with wifi direct, but neither even can show a wlan0 interface. In the past I have used a DK2 with buildroot and got the wlan0, and a coworker used stock yocto build on the DK2 a...

BillR by Associate III
  • 605 Views
  • 1 replies
  • 0 kudos

NETDEV WATCHDOG: eth0 (cpsw): transmit queue 0 timed out

Hi:​Anyone familiar with this issue?When I plug in the network cable, the following information will be printed later:​[ 373.607360] ------------[ cut here ]------------[ 373.610551] WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:447 dev_watchdog+...

Wjian.1 by Associate II
  • 3320 Views
  • 6 replies
  • 0 kudos